Better performance.
Less energy.
Ants can build hills. Cheetahs can accelerate as fast as sports cars. People can reach for the stars. All it takes is the right amount of energy at the right time, which means using energy efficiently as well as saving it when you don’t need it.
As the world transitions to greater reliance on electricity, the opportunity is to apply the right amount of energy at the right time. ABB drives together with electrical motors could deliver such efficiencies of energy use up to 80%.